The Perkins® 1500 Series is engineered to provide class leading performance and maximise competitive advantage for our customers. The 1506 is a 6 cylinder, fully electronic, turbocharged, air-to-air aftercooled diesel engine. It is economical, quiet, reliable, and provides the high performance that is demanded by our customers for their power generation needs. Furthermore, the ElectropaK comes as a complete unit, fitted with features such as the radiator pack, the air cleaner, and all of the wiring harnesses needed for convenient installation.
| Gross Mechanical Output | 192-358 kWm |
| Typical Electrical Output | 207-389 kVA (166-312 kWe) |
| Emissions | Fuel Optimised |
A great feature of the series is the ease with which users can move between 50-60 Hz power frequencies. So if you're a rental company shipping from Lebanon to Saudi Arabia, for example, you just flick a switch to meet local standards. There's no technician to call, making life easier for you and the operator.
All the engines in the 1500 Series benefit from our electric power warranty of one year unlimited hours or two years with up to 500 hours use per year. Your engine will also be supported by our highly trained global distributor network, who will ensure it keeps running whenever and wherever it's used.The 1500 Series in designed to provide low cost of ownership, simple maintenance and reduced downtime. Oil change intervals are set at 500 hours as standard. One of its most impressive benefits is a fuel saving of up to seven percent on previous models. This is significant in terms of reducing ownership and operating costs. In fact, five to seven years of fuel savings at this level will pay for the entire cost of the engine.
Our 1500 Series has world-class power density that is achieved using a hydraulic actuated unit injection (HEUI) fuel system. This makes the engine robust enough for any territory as it can cope with the variation in fuel quality around the world. The engines are also designed to provide reliable power even in the most extreme climates and performed above and beyond expectations in ambient testing. It also has an improved capability of up to eight percent at altitude making it a durable and dependable performer.
| Gross Mechanical Output | 192-358 kWm |
| Typical Electrical Output | 207-389 kVA (166-312 kWe) |
| Rated Speed | 1500/1800 rpm |
| Prime | 207-308 kVA |
| Standby | 228-337 kVA |
| Prime | 166-282 kWe |
| Standby | 218-312 kWe |
| Emissions | Fuel Optimised |
| Number of Cylinders | 6 vertical inline |
| Bore | — |
| Stroke | — |
| Displacement | — |
| Compression Ratio | 16.1:1 |
| Aspiration | Turbocharged aftercooled |
| Combustion System | Direct injection |
| Rotation from Flywheel End | Anti-clockwise |
| Cooling System | Liquid |
| Aftertreatment | - |
| Typical Alternator Efficiency | 92% |
| Switchable | Yes |
| Length | — |
| Width | — |
| Height | — |
| Dry Weight | — |
| Note 1 | *Final dimensions dependent on selected options |
| Prime Power | Variable load. Unlimited hours usage with an average load of 70% of the published prime power rating. A 10% overload is available for 1 hour in every 12 hours of operation. |
| Standby Power | Variable load. Limited to 500 hours annual usage up to 300 hours of which may be continuous running. No overload is permitted. |
A great feature of the series is the ease with which users can move between 50-60 Hz power frequencies. So if you're a rental company shipping from Lebanon to Saudi Arabia, for example, you just flick a switch to meet local standards. There's no technician to call, making life easier for you and the operator.
All the engines in the 1500 Series benefit from our electric power warranty of one year unlimited hours or two years with up to 500 hours use per year. Your engine will also be supported by our highly trained global distributor network, who will ensure it keeps running whenever and wherever it's used.The 1500 Series in designed to provide low cost of ownership, simple maintenance and reduced downtime. Oil change intervals are set at 500 hours as standard. One of its most impressive benefits is a fuel saving of up to seven percent on previous models. This is significant in terms of reducing ownership and operating costs. In fact, five to seven years of fuel savings at this level will pay for the entire cost of the engine.
Our 1500 Series has world-class power density that is achieved using a hydraulic actuated unit injection (HEUI) fuel system. This makes the engine robust enough for any territory as it can cope with the variation in fuel quality around the world. The engines are also designed to provide reliable power even in the most extreme climates and performed above and beyond expectations in ambient testing. It also has an improved capability of up to eight percent at altitude making it a durable and dependable performer.
Data not available.