1506A-E88TAG2024-02-05T16:41:28-06:001506A-E88TAG1506A-E88TAG Electric Power Diesel EnginePerkinsCurrentAir inlet systemMounted air filter and turbochargerCooling systemAir-to-air charge cooler incorporated in radiatorMounted belt driven pusher fanRadiator supplied loose with all guards and pipesThermostatically controlled with belt driven, circulating pump and belt-drive fanElectrical equipment24 volt starter motor and 24 volt 45 amp alternator with DC outputECM mounted on engine with wiring looms and sensorsFlywheels and flywheel housingAluminium SAE 1 flywheel housingHigh inertia flywheel to SAE 1 J620 Size 355.6 mm (14 in)Fuel systemElectronic governing to ISO 8528-5 with stand-alone isochronous and load-sharing capabilitiesFuel filter, fuel transfer pump, fuel priming pumpHEUI fuel system with full authority electronic controlSpin on primary, secondary and water filter separatorMountingsFront engine mounting bracketOil systemFull flow spin-on filtersOil pump gear drivenWet full aluminium sump with filler and dipstickFind your distributorhttps://www.perkins.com/distributorMicrosite1Operation and Maintenance Manualhttps://www.perkins.com/manualsMicrosite2Greater functionalityA great feature of the series is the ease with which users can move between 50-60 Hz power frequencies. So if you're a rental company shipping from Lebanon to Saudi Arabia, for example, you just flick a switch to meet local standards. There's no technician to call, making life easier for you and the operator. <p ></p> All the engines in the 1500 Series benefit from our electric power warranty of one year unlimited hours or two years with up to 500 hours use per year. Your engine will also be supported by our highly trained global distributor network, who will ensure it keeps running whenever and wherever it's used.Lower operating costsThe 1500 Series in designed to provide low cost of ownership, simple maintenance and reduced downtime. Oil change intervals are set at 500 hours as standard. One of its most impressive benefits is a fuel saving of up to seven percent on previous models. This is significant in terms of reducing ownership and operating costs. In fact, five to seven years of fuel savings at this level will pay for the entire cost of the engine.Performance you can rely onOur 1500 Series has world-class power density that is achieved using a hydraulic actuated unit injection (HEUI) fuel system. This makes the engine robust enough for any territory as it can cope with the variation in fuel quality around the world. The engines are also designed to provide reliable power even in the most extreme climates and performed above and beyond expectations in ambient testing. It also has an improved capability of up to eight percent at altitude making it a durable and dependable performer.1506A-E88TAG Electric Power Diesel Engine1506A-E88TAG Electric Power Diesel Engine
1506A-E88TAG Electric Power Diesel Engine
1506A-E88TAG1-2-3-4-5 ElectropaK Specification Sheet1506A-E88TAG1-2-3-4-5 ElectropaK Specification SheetGenerator Set Power Selector ChartGenerator Set Power Selector Chart360° Exterior View (HTML)
360° Exterior view. Double click on the image to zoom in on any area of the product
Power RangeTotal Power RangeGross Mechanical Output192-358 kWmTotal Power RangeTypical Electrical Output207-389 kVA (166-312 kWe)Total Power RangeRated Speed1500/1800 rpm50 Hz Typical Electrical OutputPrime207-308 kVA50 Hz Typical Electrical OutputStandby228-337 kVA60 Hz Typical Electrical OutputPrime166-282 kWe60 Hz Typical Electrical OutputStandby218-312 kWeEmission StandardsEmissionsFuel OptimisedGeneralNumber of Cylinders6 vertical inlineGeneralBore4.4in112mmGeneralStroke5.9in149mmGeneralDisplacement537in³8.8lGeneralCompression Ratio16.1:1GeneralAspirationTurbocharged aftercooledGeneralCombustion SystemDirect injectionGeneralRotation from Flywheel EndAnti-clockwiseGeneralCooling SystemLiquidGeneralAftertreatment-GeneralTypical Alternator Efficiency92%GeneralSwitchableYesElectropaK DimensionsLength76.4in1941mmElectropaK DimensionsWidth39.9in1013mmElectropaK DimensionsHeight53.8in1366mmElectropaK DimensionsDry Weight2549lb1156kgDisclaimerNote 1*Final dimensions dependent on selected optionsDefinitionsPrime PowerVariable load. Unlimited hours usage with an average load of 70% of the published prime power rating. A 10% overload is available for 1 hour in every 12 hours of operation.DefinitionsStandby PowerVariable load. Limited to 500 hours annual usage up to 300 hours of which may be continuous running. No overload is permitted.The Perkins® 1500 Series is engineered to provide class leading performance and maximise competitive advantage for our customers. The 1506 is a 6 cylinder, fully electronic, turbocharged, air-to-air aftercooled diesel engine. It is economical, quiet, reliable, and provides the high performance that is demanded by our customers for their power generation needs. Furthermore, the ElectropaK comes as a complete unit, fitted with features such as the radiator pack, the air cleaner, and all of the wiring harnesses needed for convenient installation.The Perkins® 1500 Series is engineered to provide class leading performance and maximise competitive advantage for our customers. The 1506 is a 6 cylinder, fully electronic, turbocharged, air-to-air aftercooled diesel engine. It is economical, quiet, reliable, and provides the high performance that is demanded by our customers for their power generation needs. Furthermore, the ElectropaK comes as a complete unit, fitted with features such as the radiator pack, the air cleaner, and all of the wiring harnesses needed for convenient installation.PerkinsFuel Optimized1500 SeriesFuel Optimized181-300 kWm301-600 kWmDieselEP Diesel1506A-E88TAG11506A-E88TAG21506A-E88TAG31506A-E88TAG41506A-E88TAG5Electropak2024-02-05T16:41:28-06:00